Notifications

warning

unintended equipment operation

Do not rely solely on Notifications Settings for alarm notifications where human or equipment safety relies on successfully delivered notifications.
Do not use Notifications Settings for critical control or protection applications where human or equipment safety relies on the operation of the control circuit.
Consider the implications of unanticipated transmission delays or failures of communications links.

Failure to follow these instructions can result in death or serious injury.

NOTE: Other parts of the overall communication system, such as email servers and cellular phone systems, could fail and result in notifications not being delivered. If notifications are not delivered to recipients, conditions that cause alarming may persist and result in safety critical issues.

 

Notifications alert specific people in your facility about critical power incidents no matter where they are. Notifications deliver timely alerts of power system events to the mobile phone, email or pager of designated users and helps them quickly identify system abnormalities and take appropriate action.

Notifications provide:

  • View-based alarm grouping
  • Basic and custom alarm filtering
  • Flexible notification schedules
  • SMS and email notification relay
  • Primary and Standby Alarm Server synchronization
  • Maintenance mode

Notifications Settings accepts alarms for the Power Operation Alarm Server. Notifications Settings alerts specified recipients based on the configured notification.

Subsequent topics explain how to configure and maintain your system notifications.

Topics in this section: